Non section component in a view and Crosshatch settings.

2021-10-06T23:27:39Z

Summary


Details

If two bodies are overlapping in a section view, you don't want to see the crosshatching in the intersection area. 

Solution

Therefore you can use the function "Section in View" to display bodies or components as "make as non sectioned". that the crosshatch normaly not correct.

MB3 the View Style and switch on Section - Settings - "Process hidden Crosshatch"
That should be fixed the crosshatch overlaping .


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1899
Function: DRAWING/VIEW

Ref: 002-8171727

KB Article ID# PL8171727

Contents

SummaryDetails

Associated Components