Tecnomatix Credentials for database association during Upgrade

2021-10-07T00:01:53Z
eM-Server

Summary


Details

Is there a way to maintain or carry forward the credentials used to associate to the Oracle Schema during the process of moving from version 14.1.2 to 15.1 (or any upgrade)?



Solution

If the schema and its password is not changed, then the eMS_config.cfg file of Tecnomatix 14.1.2 can be opened, which is located in the folder pointed to by: Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Tecnomatix\eM-Planner\Settings\CnfgFolder

The encrypted value of Password field can be copied and pasted into the eMS_config.cfg file of Tx 15.1. 

The whole eMS_Config file can be copied from Tx 14.1.2 to Tx 15.1 as well.



Notes and References


Hardware/Software Configuration

Platform: na
OS: all
OS Version: n/a
Product: TECNOMATIX
Application: EM-SERVER
Version: V15.1
Function: ADMIN_TOOLS

Ref: 001-9746116

KB Article ID# PL8171567

Contents

SummaryDetails

Associated Components

eMS AdminConsole