Workflow:
- User opens a Solid Edge draft in SEEC that is created from a Family of Parts member
- Save as Translated
- The following message appears
Since the user wants to create a DXF of the single draft the message is not relevant to their task.
Solution
This is a known issue and fixed in Solid Edge 2021.
There is a workaround for this issue: do not load the linked 3D parts to your SEEC cache
Steps to perform:- Start with an empty SEEC cache
- File Open
- Check "Open options" - verify that the Download options are off

- Set Load Option to "Inactive drawing views for review"
If you check the SEEC cache only the draft is now in the cache
Save as Translated will now open the dialogue:
A second workaround is to delete the linked 3D files from cache before the Save a Translated action.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP11
Function: SEEC
Ref: 002-8171471