NX Spot drilling depth issue - "The Spot drill depth is too large to machine with the selected Cutter"

2021-10-06T23:27:39Z
NX for Manufacturing

Summary


Details

Spot drilling operation - manually setting the depth of cut may give an Alert: "The Spot drill depth is too large to machine with the selected Cutter"



Solution

The Depth of a spot drilling operation is limited to twice the 'Point Length' (PL) of the tool. If this is exceeded, then the Alert is given.



Notes and References


Hardware/Software Configuration

Platform: na
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V1919
Function: DRILLING

Ref: 001-9744072

KB Article ID# PL8171466

Contents

SummaryDetails

Associated Components

Manufacturing General