Assembly sent from Teamcenter Structure Manager to NX is not loading any child components
When an assembly is being sent to NX from Teamcenter Structure Manager by highlighting just the assembly line, the result of the NX load shows only the selected assembly file is loaded; all its children components are not loaded. This behavior is different when compared to loading the assembly from My Teamcenter, which follows the Assembly Load Options selected in NX.
Solution
The following Teamcenter preferences determine how the assembly is loaded in NX from Teamcenter Structure Manager:
BOMWriterNoDescendantsInPLMXMLDetermines whether descendants (children and grandchildren) of selected BOM lines are included when NX is launched from Teamcenter Structure Manager.
Set to
TRUE: descendants are not included.
Set to
FALSE: descendants are included.
Default is
TRUE.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: TC_PORTAL
Ref: 001-9732639