Wave linked object colors don't display color of parent

2021-10-06T23:27:39Z

Summary


Details

Linked objects won't update to new parent colors. After creating a linked object and then going back to the parent part and editing the color of the parent object, the linked object does not automatically update.



Solution

This is as Designed.
The option for "Use Display Properties of Parent Part" Color propagation is for create or edit only and will not update on-the-fly or automatically. 
To Update the Linked object color to the Parent object color:
1. Right click on the linked feature to edit.
2. Toggle the option for "Use Display Properties of Parent Part" Off then back On and the color of the linked object will update to the parent objects new color. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: WAVE

Ref: 001-9732534

KB Article ID# PL8171463

Contents

SummaryDetails

Associated Components