The Diagnostic tool keeps giving an error about the Schema path although configuration of Fast Search seems to be correct and the Custom properties are listed in the Fast Search tool.
Error:
Solution
Solution
The BuiltInDiagApp.exe verifies the values of two regkeys.
Please check the values of these two regkeys:
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\PropertySystem\PropertySchema\0001 for the SEUser.propdesk
And
Computer\HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\PropertySystem\PropertySchema\0000 for the seprops.propdesc
Both should match with the Fast Search config.
In this example, both regkeys had multiple values (and paths) for the seprops.propdesc and SEUser.propdesk. After removing the wrong values the Diagnostic tool will not report an error.
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP5
Function: SEDM
Ref: 002-8171094