Assembly is selected in Structure Manager to send to NX, but none of the components are loaded

2021-10-06T23:27:39Z

Summary


Details

When an assembly is selected in Structure Manager to send to NX, none of the components are loaded into NX. Only the top level is loaded with its structure.

Solution

In Teamcenter, select 'Edit-->Options'.
Set the following Teamcenter preference to the value, "FALSE" (without the double quotes).

BOMWriterNoDescendantsInPLMXML
Determines whether descendants (children and grandchildren) of selected BOM lines are included when NX is launched from Teamcenter.
If set to TRUE, descendants are not included. If set to FALSE, descendants are included. Default is TRUE.



Notes and References

In Structure Manager, if an assembly is selected to send to NX, none of the subassembly components are loaded into NX. This does not follow the documentation found at:
 https://docs.plm.automation.siemens.com/tdoc/nx/1899/nx_help/#uid:xid1494159
Which states that selecting the assembly implies selecting all its decendents.
A note with the information that the above Teamcenter preference needs to be set to allow this functionality, will be added to the NX1926 Help documentation.
 



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 002-8171092

KB Article ID# PL8171092

Contents

SummaryDetails

Associated Components