Meaning for the below message in FEMAO
"Due to external points not being visible through AML, domain detection for this AML is significantly slower"
Solution
If the microphones in the model are not caught by AML, then such message will be there.
For example if there are microphones behind a symmetry plane or at locations where AML cannot access?If so, removing those microphones might help.
In any case, those microphones will be resulted as zero pressure.
Notes