User extract contact force of a particular face for surface-to-surface Glue contact in SOL 402 run ?
Solution
BGRESULTS output request is not supported for SOL 402, however user can request MPC forces in Simcenter GUI itself in case control.
After solving, in result file, user can confirm the reaction force MPC.
If the user's interest is to know contact fore for one particular face , then he can use 'identify" command in post processing and "feature face" in pick . Here user can find Sum of all nodes in that selected face.
Notes