Simcenter 3D Solutions What is the default value UGII_CAE_POST_TEMPLATE_USER_DIR ?

2021-10-06T23:27:38Z
Simcenter 3D

Summary


Details

If the user had not defined UGII_CAE_POST_TEMPLATE_USER_DIR as a Env Variable in the machine, then what is the default value  of Env Variable UGII_CAE_POST_TEMPLATE_USER_DIR ?

Solution

When the user doesn't specify the ENV variable in OS , then it is taken from ugii_env_ug.dat file inside "Installation directory/UGII folder" with the following content in this file.

UGII_CAE_POST_TEMPLATE_USER_DIR=${HOME}\post_template_files

and the default value for Home

HOME=${TMP}

Hence it will take %TMP% location if user doesn't specify intentionally.

Infact user is having the option to either set in OS or set in ugii_env.dat file.

Notes

KB Article ID# PL8171023

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow