Quick View Cube is not shown even Show Quick View Cube in window is checked?

2021-10-06T23:57:03Z

Summary


Details

Quick View Cube is not shown even Show Quick View Cube in window option is checked.

Solution

On Quick View Cube Settings dialog check the value for 'Reduce opacity when not in focus'. If it is set to '0' then Quick View Cube will be completely transparent in the inactive state.


'Quick View Cube Settings' are available in Solid Edge Options-View Tab.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V220MP5
Function: UI

Ref: 002-8171007

KB Article ID# PL8171007

Contents

SummaryDetails

Associated Components