Solid Edge How can I Show construction geometry when placing parts that do not have a design body?

2021-10-06T23:57:02Z
ASSEMBLY

Summary


Details

How can I Show construction geometry when placing parts that do not have a design body?

Solution

From Solid Edge Option assembly tab under 'Construction Display Options when Placing Component' check option 'Show construction geometry when placing parts that do not have a design body'.


When checked, display the construction geometry for a part that does not have a design body. If there are construction surfaces in the part, show construction surfaces, if there are no construction surfaces then show construction curves, if there are no construction curves and surfaces then show sketches, and if none of the above, then show the co-ordinate system associated with the part (this will override the option to show/hide coordinate system). This is checked by default.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V220MP5
Function: COMPONENTS

Ref: 002-8170986

KB Article ID# PL8170986

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS