NX About "Legacy" in customer default (Teamcenter intergation-->general-->feature-->weld publishing method).

2021-10-06T23:27:38Z
NX for Design

Summary


Details

Publish to TC doesn't works if turn on this "Legacy" in customer default (Teamcenter integration-->general-->feature-->weld publishing method).





Solution

Publish to TC works fine if turn off option "Legacy" in customer default (Teamcenter integration-->general-->feature-->weld publishing method).

Information related to the "legacy".
 
The legacy publishing is design in previous NX version(before NX9), it is publishing weld feature as psOccurence, one type of weld feature will shared with one item,  the feature didn't have item id and lifecycle etc.
 
If turning off legacy publish, that will enable item-based publishing, which is new publishing method delivered from NX9. Each weld feature will be published as item, the feature will have unique id and lifecycle etc. 

Notes and References

9000649

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: KDA
Version: V11.0.2
Function: WELD_ASSISTANT

Ref: 002-8170963

KB Article ID# PL8170963

Contents

SummaryDetails

Associated Components

Modeling