"Adding item numbering rules" capability

2021-10-06T23:27:38Z

Summary


Details

"Adding item numbering rules" not working in File > New dialog, defined multiple naming rules are visible, but on applying particular naming rule, only default naming rule is getting applied. 

Solution

"Adding item numbering rules" requires new TC SOA service, which is not available in TC10.1.7.

In TC 10.1.7, we do not use generateNextValues SOA and hence, it is not possible to specify the Naming Rule values as an input to the generation of the Item_id.
However, the item_id that gets generated is still correct and the user (although cannot specify the input naming rule) can still know what the active naming rule is which will be used to generate the item_id.

TC11.0.x is when we started using the new SOA that will allow the naming rule functionality to be used to its fullest

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_NEW

Ref: 002-8165786

KB Article ID# PL8165786

Contents

SummaryDetails

Associated Components