Details
A studio spline is created using a set of through points.
When trying to extract those points from the spline using 'points set->Definition points' , an error message is displayed claiming that the spline does not have definition points.
How to create a spline curve that have definition points?
Solution
Defining points are the points through which the spline is created.
Number of through points must be greater than the degree of the spline to have defining points extracted
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: STUDIO_DESIGN
Version: V1899
Function: FREE_FORM
Ref: 002-8165774