NX Geometry created with "Symmetric Modeling" in NX Realize Shape is not connected smoothly

2021-10-06T23:27:38Z
NX for Design

Summary


Details

The body created with "Symmetric Modeling" in NX Realize Shape is not connected smoothly.


How to create smoother resultant body with C2 continuity?



Solution

If the user selects symmetry plane exactly at the edge of the base body,


then it could create sharp edges based on the angle of the adjoining faces.


The user needs to select a symmetry plane that intersects with  base body for getting smoother surface with C2 continuity. 


As a workaround for such specific cases, the user can execute "Set Continuity" for getting smoother continuity.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: STUDIO_DESIGN
Version: V1872
Function: SUBDIVISION

Ref: 002-8165750

KB Article ID# PL8165750

Contents

SummaryDetails

Associated Components

Modeling