NX The spherical body is not displayed in Lightweight Representations.

2021-10-06T23:27:37Z
NX for Design

Summary


Details

When using Lightweight Representations and "Partially Shaded" or "Static Wireframe", the spherical body is not displayed.

Solution

There is logic that no matter how the silhouette toggle is set (on/off) that the first draw will treat the silhouettes as model edges and render them.  This only applies to the initial draw.  When the silhouettes are turned ON, no change.  When they are turned OFF, the silhouettes are deleted and in the case of a simple sphere, there is no image.  

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1809
Product: NX
Application: ASSEMBLIES
Version: V1899
Function: ASSEMBLY_MODEL

Ref: 002-8035631

KB Article ID# PL8035631

Contents

SummaryDetails

Associated Components

Assemblies