NX How to add new property in NX manager File new dialog

2021-10-06T23:27:37Z
NX for Design

Summary


Details

How to add new property in NX manager File new dialog



Solution

In the file new dialog new property can be added using operation descriptor or attribute mapping.


Operation descriptor - In Teamcenter, you can add operation descriptors to a business object in the BMIDE, such as Item, Item Revision, Item Master Form, and so on, to let you customize the inputs that are collected based on the operation performed, such as creating a new part or performing a Save As on an existing part.


The operation descriptors consist of creation descriptors and Save As descriptors defined in Teamcenter on the CreateInput and SaveAsInput tabs for the business object. 


When you add Teamcenter operation descriptors, these are reflected in NX where you need to input values for these properties when you are creating an object


Attribute mapping - In the attribute mapping if "/required" is added for the UGMASTER property then it will show in the file new dialog.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1899
Function: FILE_NEW

Ref: 002-8018016

KB Article ID# PL8018016

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX