Want to know about Customer Default "Synchronize settings from Teamcenter to NX".

2021-10-06T23:27:37Z

Summary


Details

Want to know about Customer Default "Synchronize settings from Teamcenter to NX".

Solution

Customer default "Synchronize settings from Teamcenter to NX" does Session sharing allows information about changes in group and role settings to be synchronized between NX and Teamcenter.
 


Customer default "Synchronize settings from Teamcenter to NX" is available from NX 1859 and later versions.
 In NX 12 environment variable UGII_DISABLE_EVENT_SHARING_WITH_RAC was available. This variable is disabled by default with Customer default "Synchronize settings from Teamcenter to NX" .
 To be synchronized means if any group or role is changed in Teamcenter with the above environment variable, in NX side also it gets synchronized.
 Ex: if Engineering group default item is "Item" and Group1 group default item is "Design"
 NX is launched when the group is set to Engineering

 Now in TC if the Group is changed to Group1 where the default is Design then NX session should automatically sync Design Item. 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1859
Function: ASSEMBLY

Ref: 002-8018015

KB Article ID# PL8018015

Contents

SummaryDetails

Associated Components