NX Need to publish Item name and number automatically in 3D PDF in NX Manager

2021-10-06T23:27:37Z
NX for Design

Summary


Details

In NX manager currently it is not possible publish Item name and number of that component  automatically. Need to enter manually during publishing the 3D PDF.

Solution

To use part attributes inside a template part, insert a static text instead of inserting a user defined text or a controlled text. 
 
 The text input for the static text should map to the part attribute that you want to retrieve in the part you are publishing.
 
 During publish, NX will automatically look up the part attribute values in the publish part and use them to populate the static text.
 
Add the properties to template part file using Menu -> File -> Properties. 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: TECH_DATA_PKG
Version: V1899
Function: PUBLISH

Ref: 002-8018013

KB Article ID# PL8018013

Contents

SummaryDetails

Associated Components

Modeling