NX Wrong IPW position (Update Local IPW from Source)

2021-10-06T23:27:37Z
NX for Manufacturing

Summary


Details

Update Local IPW from source shows In Process Workpiece (IPW) is created in the wrong position.



Solution

It is important that that the positioning type setting (Part or CSYS) is the same in the source and target workpieces, otherwise the IPW will be incorrectly positioned. 
If they have already been defined differently, then the IPW must be removed from the list in the 'Blank Geometry' form, and then be recreated.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V1919
Function: WORKPIECE

Ref: 001-9730251

KB Article ID# PL8018011

Contents

SummaryDetails

Associated Components

Manufacturing General