New operation type 'Planar Deburring' doesn't create an operation

2021-10-06T23:27:37Z

Summary


Details

Steps to duplicate incident:
  • Selection of "'reate Operation' 
  • Select "Type"--> "mill_planar"
  • Operation Subtype: "PLANAR_DEBURRING"
The selections above do not create an operation. 

Solution

Select File-->Utilities-->Feature Toggles...

Select MfgCore_PlanarDeburring and change the "State" to "On"  (MouseButton3 on "State" and switch to "On").

Operation dialog box is seen in the image below...


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: P1926
Function: PLANAR_DEBUR

Ref: 002-8018005

KB Article ID# PL8018005

Contents

SummaryDetails

Associated Components