The previous release dialog boxes are displaying when creating 'Blank Geometry'.

The NX1926 updated dialog boxes can be seen in the image below...

Solution
- Select File-->Utilities-->Feature Toggles...

- Select MfgCore_CreateBlankComponent
- Change the State to On (MB3 in the field for State).
Updated dialog boxes can be seen in the image below...
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CAM
Version: P1926
Function: WORKPIECE
Ref: 002-8018004