NX Changing the A and B angle step sizes in CMM Inspection

2021-10-06T23:27:37Z
NX for Manufacturing

Summary


Details

When defining a sensor it is only possible to set the A angle in multiples of 7.5 degrees.
Is there any way to change the default angle step size?

Solution

Right-click on the SENSORS folder, select Properties and create these attributes:

A ANGLE STEP SIZE
B ANGLE STEP SIZE

For example:

Now the A angle can be set in multiples of 5 degrees instead:


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: CMM_INSPECTION
Version: V1903
Function: OTHER

Ref: 002-8017651

KB Article ID# PL8017651

Contents

SummaryDetails

Associated Components

Manufacturing CMM