Software version:
=================
NX12 and higher
This document is actual for customers, which use ESKD standard for drafting.
ESKD limit values are incorrect for the following tolerances: F5, F6, F7, F8, F9
These values are contained in the following file:
UGII\drafting_standards\eskd\lim_fits_table_data_eskd_1.txt
Solution
Existing ER_9692636 describes this issue.
Today we can suggest the following 2 Workrounds for customers, which use ESKD standard for drafting:
1) According to the GOST 25346-2013, tolerance values in ESKD Standard correspond to ISO Standard.
So customers can change "Drafting Standard\General\Limits and Fits" Customer Default option to ISO, and NX will use ISO file which is located at the "...UGII\drafting_standards\iso".

2) Neighboring "iso" folder contains file with correct values, corresponding to ESKD standard:
UGII\drafting_standards\iso\lim_fits_table_data_iso_1.txt
Open lim_fits_table_data_iso_1.txt file in Text Editor and "Save" it as lim_fits_table_data_eskd_1.txt.
Put this file to "UGII\drafting_standards\eskd" folder instead of incorrect OOTB file.

Notes and References
ER_9692636
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: DIMENSION
Ref: 002-8017639