How to publish JT data at the time of Importing NX part files

2021-10-06T23:27:37Z

Summary


Details

How to publish JT data ate the time of Importing NX part files?



Solution


When you import parts into the Teamcenter database, you can now select the Publish JT Data option to publish JT data.



When the option is selected, the Publish Optional Information option is automatically selected also, which enables the JT data to be published.



You must select the Publish JT Data option before you identify the items for import, such as an assembly or an import from a folder. Otherwise, the option is unavailable.




If you are using "tcin_import.exe" utility for importing the data, then you can use below options for publishing the JT-


-publish_information=yes 
-publish_jt=yes


 | Note | Publish JT Data is not applicable for CAE parts, but you can still publish JT data asynchronously for CAE parts during import by selecting the Save JT Data option in the Save Options dialog box.



Notes and References

9708451



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V1847
Function: CLONE_IMPORT

Ref: 002-8017610

KB Article ID# PL8017610

Contents

SummaryDetails

Associated Components