What variable is used in
Post Builder to report the
Tracking Point X and
Y Offset from a
Turning Tool. There may be more than one variable that can be used. Which variable is preferred.

Solution
The
mom_tool_offset() is the suggested variable to read these settings. It may be necessary to check to see if
mom_tool_offset_defined is set to 1 before using
mom_tool_offset.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1903
Function: POSTBUILDER
Ref: 001-9722001