Simcenter 3D Solutions Multiple directories are defined by UGII_CUSTOM_DIRECTORY_FILE

2021-10-06T23:27:36Z
Simcenter 3D

Summary


Details

Which root directory is used if Multiple directories are defined by UGII_CUSTOM_DIRECTORY_FILE ?

Solution

The environmental variable UGII_CUSTOM_DIRECTORY_FILE defines the fullpath to a file containing a list of root directories for custom applications.  NX will use the first instance of the custom application it finds.

Example 1:  NX finds the custom application in first listed root directory.  NX does not search any more root directories.

Example 2:  NX does not find the custom application in the first listed root directory.  NX proceeds to the next root directory and continues on in the listed order.

Notes

KB Article ID# PL8017537

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow