Keep Solid Edge data linked to Excel on Teamcenter

2021-10-06T23:56:58Z

Summary


Details

How to maintain link between Excel and Solid Edge Part in Teamcenter



Solution

When create part with using excel values and checkin, it creates excel dataset and SE dataset under the same item revision, excel will be uploaded and copied to SEEC cache.


And that will be the duplicate copy of Excel in the SEEC cache and has no link with original excel in TC RAC.


Yes the link with original excel breaks.


Excel on Teamcenter is not updated as the SE part will be referring the excel from SEEC cache.



Notes and References

IR 9634049

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 002-8017408

KB Article ID# PL8017408

Contents

SummaryDetails

Associated Components