Thermal and Flow solver update for NX

2021-10-07T00:09:05Z

Summary


Details

Siemens PLM is pleased to inform you that the latest version of the Thermal and Flow solvers is now available for download from the Siemens PLM Download server. For details of patches included with this release please see the associated README.pdf file included with the release. This README file also includes instructions for installing this update. 
            
This release contains updates for NX 1872 series, 1899 series, and 1926 series. To download the update, start at the Siemens Support Center site. Note a valid WebKey account is required for download. 
             
Once on Support Center select downloads. 


  1. Select the desired version.
  2. Select Add Ons. 
  3. On the left column, select he desired OS and "Thermal and Flow". 
Download the updated installation kit 

SFB-NX-8520249
Product Information:
  • Product: NX , Application: CAE , Version: V1926

KB Article ID# PL8520249

Contents

SummaryDetails

Associated Components