The following errors occurred during the SEEC "Check In" operation.
"part name" | Each document can only be processed by one transaction at a time. Wait for the current transaction to complete and then try again.
Could not check in a part due to settings in the Solid Edge options file. The options file is shared by all users; however, the SEEC Cache setting was referencing a single user.
Solution
In this use-case, the users could not check in a part due to settings in the Solid Edge options file. The Options file is shared by all users; however, the SEEC Cache setting references a single user.
First, to clear the check in failure message, delete the SEECTransLog.xml file in the user's SEEC Cache folder.
Now, set the value for the SEEC Cache in the Options file as follows:
<OptionName name="SEEC cache"><Value>$Default</Value><Override>No</Override></OptionName>
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 10_1903
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP6
Function: SEEC
Ref: 001-9701703