Simcenter 3D Solutions Setting Default Assembly Load Options

2021-10-06T23:27:36Z
Simcenter 3D

Summary


Details

By default, the load options for a Simcenter 3D model are set to Minimum Load - Lightweight Display. While this is beneficial for performance, some functionality and fidelity is removed by opening models this way. This also is not always clear when opening models from a file explorer window or from the History Navigator.

Solution

You can change the default loading options by going to File->Assembly Load Options as soon as you open Simcenter 3D (with no model open)

 


You can then change your load option under Scope and save the setting to a *.def file using the Save to File button at the bottom of the dialog box.


 

After this, create an environment variable called UGII_LOAD_OPTIONS and set it to point to the *.def file that was just created.


 

Then close and reopen Simcenter and your default load options should be set. 

Notes

KB Article ID# PL8017295

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow