Controlling the Teamcenter real property name row in the SEEC Common Property dialog

2021-10-06T23:56:54Z

Summary


Details

How do you control the display of the Teamcenter real property name row in the SEEC Common Property dialog (CPd)?  Do not want the Teamcenter real property names displayed on the SEEC Common Property dialog.  Want the Teamcenter display name displayed in the SEEC CPd.

Solution

 This is controlled by the Teamcenter preference "tc_display_real_prop_names" value.  A value of "0" will cause the Teamcenter real property names row to display.  Setting the value to "1" will turn off this display  and only show the Teamcenter display name.

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V219MP9
Function: SEEC

Ref: 002-8017201

KB Article ID# PL8017201

Contents

SummaryDetails

Associated Components