SEEC: message of Solid Edge file extension default item type is invalid.

2021-10-06T23:56:54Z

Summary


Details

When first opening a file after a log in, a message is displayed that a default Item Type is not valid.



Solution

This occurs when a value for the specific file type such as par, asm, dft, etc. is listed in the corresponding preference but is not listed as a value in the SEEC_Default_Item_Type preference. 
For example, the message references .asm. So we review the SEEC_itemTypeList_SE Assembly preference and find a value, Design. However, Design is not a value in the SEEC_Default_Item_Type preference, hence  the informational message is issued. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1903
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 001-9695726

KB Article ID# PL8017187

Contents

SummaryDetails

Associated Components