Solid Edge Help Collection Server does not work with F1 key

2021-10-06T23:56:53Z
PART/SHEETMETAL

Summary


Details

The Help Collection Server does not work with F1 and reports a message: 

No Documentation was found for: Deliverable
Documentation Path: /se/220/se_help 
Path: http://localhost:8282/tdoc/se/220/se_help 



Solution

The Help Collection installation will install a 2020 collection folder and this folder must be used in the Helpers Path. 

The paths to add in the Solid Edge Options Helpers Tab are

http://localhost:8282/tdoc/se/2020/se_help for a local setup

Or 

http://your_server_address/tdoc/se/2020/se_help/#uid:index for a server setup. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: HELP
Version: V220MP4
Function: OTHER

Ref: 001-9678223

KB Article ID# PL8017184

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES