NX Content Migration Manager for I-deas: Sketch Dimensions and Constraints are not migrated

2021-10-07T00:08:49Z
NX Design Translators

Summary


Details

Issue
When migrating parts from I-deas to NX, the sketch dimensions and constraints will be lost. 

Messages similar to the following can be found in the migration reports:


     "0 out of 0 constraints are converted within NX Sketch Feature "

The migration of the part should complete normally and generate an NX part that is valid for ongoing work in NX and for further migration of parent assemblies and drawings.

Solution:

This will be fixed in NX 1926.  In the meantime a patch for NX 1847, NX 1872 and NX 1899 has been posted under the Content Migration Manager for I-deas, product updates, patch, sketch_dimensions location.  


Workarounds:


  1. If and when a sketch needs to be modified, add the dimensions and constraints necessary to complete the change.
  2. Use Synchronous Modeling for making changes to the part.



SFB-NX-8017146
PR 9663217
Product Information:
  • Product: NX , Application: CMM

KB Article ID# PL8017146

Contents

SummaryDetails

Associated Components

Content Migration Manager