Affected releases: Teamcenter 11.6.0 Patch 7 – Patch 11
NX functional releases supporting Minimally Load
NX December 2019 functional release (NX 1899 Series) and
NX June 2019 functional release (NX 1872 Series) and
NX January 2019 functional release (NX 1847 Series) and
NX 12.0.2
Associated PR Number(s): 9639873
Resolved in: Teamcenter 11.6.0 Patch 12
Problem:
Teamcenter 11.6.0 Patch 7 introduced a defect that adversely affects assembly load performance when using Minimally Load - Lightweight Display option and Teamcenter Audit Manager was enabled.
The workaround is to turn off Teamcenter Audit Manager.
Solution:
The problem is resolved in Teamcenter 11.6.0 Patch 12.
Solution Update:
The problem documented in SFB-TEAMCENTER-8507676 is resolved in a Teamcenter 11.6.0 Patch that is higher than Teamcenter 11.6.0 Patch 12.
Determine if the problem described in the SFB-TEAMCENTER-8507676 impacts you. If it does, the solution provided in that SFB is the minimum Teamcenter 11.6.0 patch level.
SFB-NX-8017139
Product Information:
- Product: NX , Application: NXMANAGER