JT Files turn out overexposed when viewed in Teamcenter Visualization and JT2Go

2021-10-06T23:56:53Z

Summary


Details

A customer works in a managed multi-CAD environment (NX and Solid Edge). Both NX and Solid Edge create JT files that are uploaded to Teamcenter.  The NX generated JT files appear fine.  However, when a Solid Edge generated JT is uploaded to Teamcenter, these files look overexposed in Viewer and Visualization and colors seem to change during translation


Workflow: 


  • Save an unmanaged Solid Edge file as a JT file. 
  • Upload the JT to Teamcenter using Add to Teamcenter Interactive
  • Result: The JT file will appear overexposed in Visualization and Viewer


Is there something we can do to prevent the SE files from overexposing? 



Solution

The workaround for this is to edit the SePvTrn.ini. 

Change the value of the parameter below from 1 to 0:

Use Solid Edge Resolution =0 

Make sure to keep LOD settings to the default.  Changes in this value may cause different geometry. 

Default LOD settings: 

[LOD 1]Level = 1Chordal=0.001Angular=20Length=0FeatureSuppression=0Simplify=1.0AdvCompressionLevel = 0 
[LOD 2]Level = 2Chordal=0.0035Angular=0Length=0FeatureSuppression=0Simplify=0.4AdvCompressionLevel = 0.5 
[LOD 3]Level = 3Chordal=0.01Angular=0Length=0FeatureSuppression=0Simplify=0.1AdvCompressionLevel = 1 



Notes and References


Hardware/Software Configuration

Platform: na
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 001-9686201

KB Article ID# PL8017119

Contents

SummaryDetails

Associated Components