Convert very large NX Assembly to STEP AP214 produces no step file.

2021-10-06T23:27:35Z

Summary


Details

Convert very large NX Assembly to STEP AP214 produces no step file.



Solution

The reason is often, as in this Use Case, the Load Options Setttings with a value of "Minimally Load - Light Weight Display". 
Please re-execute File/Open... and on the bottom left side of this dialog, please select "Fully Load", then hit OK. 
Then re-execute the File/Export STEP command. 
If your RAM is not sufficient, please also try, inside the "Export to STEP Options" Dialog, in the Advanced TAB, to set this checkbox : 
Export Assembly as External References.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: TRANSLATOR
Version: V1899
Function: STEP_AP214

Ref: 001-9687050

KB Article ID# PL8017071

Contents

SummaryDetails

Associated Components