February 7, 2020 Dear Solid Edge Customer: Solid Edge 2019 Maintenance Pack 11 is now available for download.
Sincerely,
The Solid Edge Team =====================
Maintenance Pack Version:=====================
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
Solid Edge 2019 MP11
Version
: 219.00.11.04 ================
Download Location:================
Solid Edge 2019 Maintenance Packs can be downloaded from:
https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/ ===============
E-mail Notification: ===============
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
For details on initiating your email subscription navigate to:
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html ============================================
This Maintenance Pack addresses the following PRs:============================================
===API===PR 9578103: Need an API function for a specified ribbon tab activation
PR 9594011: HoleTable2 cell can't be overwritten via API with individual property text
PR 9616989: Delete DocumentSummayInformation empty properties
PR 9667655: AddDerivedConfig Method make SolidEdge unstable and\or crashes
PR 9645450: Draft Automation: can no longer edit a cell value in a Solid Edge Table
===General===PR 9534819: Slow sketch commands that use styles
PR 9472310: The automated crash log workflow is no longer opening the e-mail application
PR 9562554: 3YourMind service page is not able to display
===Assembly===PR 9487247: When you increase the number of pattern occurrences in an FOA it could fail
PR 9617044: Infinite crossing lines appear with accelerated sketches
PR 9513148: Error in Standard Parts when adding a custom FOP for use with Teamcenter
PR 9644137: Unable to select All Identical Parts
PR 9656532: Frame end conditions are lost when changing some dimension to sketches
PR 9657910: Not all selected components are auto simplified
===Draft===PR 9522595: Text box justification/indent settings
PR 9536180: Solid Edge freezes if Library Folder points to the Desktop and Thumbnail active
PR 9589276: Consistent crash when updating a draft
PR 9639887: enable automatic jogging for coordinate dimensions does not work
===Part/Profile/Sheetmetal===PR 8420018: Not able to modify driving dimensions
PR 9584163: Cannot Lock and adjust a dimension in the sketch profile as expected
PR 9644865: Problem with chamfer preview
===Built-in Data Management===PR 9635866: Author property is replaced by user revising files in SEDM
PR 9611845: File properties / Status tab make Solid Edge freeze for 10 minutes
===Design Manager===PR 9544830: Save As operation is slow in Design Manager
===Insight===PR 9600064: Permission error during saving as since MP9
===Teamcenter Integration for Solid Edge===PR 9539084: Active Workspace 4.2 in SEEC Drag and Drop does not work
PR 9577043: Add to Teamcenter Interactive closes when importing assembly
PR 9114269: Need to keep separate setting for TC/OS managed SAC file location
PR 9601979: Mismatch of date attributes mapped from CAD to Teamcenter.
PR 9621597: Intermittent SEEC error after starting SE
PR 9639434: SEEC Structure synchronization fails when SEEC_ExpandStructure=1
===Translators===PR 9521310: Crash when converting a DFT to DWG
PR 9577689: CAD properties disappear when converted to JT file
PR 9563723: Missing a fold extension line in the converted DWG file
SFB-SOLID_EDGE-8017040
Product Information: