How do license managers handle floating Solid Edge 2019 and floating 'Solid Edge Wiring and Harness Design' ?
Solution
If you want to remain on Solid Edge 2019 (floating) and use 'Solid Edge Wiring and Harness Design' (floating SEWIRHAR pointing to COMPOSITE id), this will work. Think of 'Solid Edge Wiring and Harness Design' as an add-in, such as FloEFD, where the license servers run independently. The license server delivered with SE2019 can serve Solid Edge 2019, and the SPLM License server can serve 'Solid Edge Wiring and Harness Design' .
Notes
If you have further inquiries about Solid Edge Solid Edge Portfolio Products Licensing please refer to the FAQs Collection link below:
Solid Edge Portfolio Products Licensing FAQs Collection