SEEC: Add to Teamcenter family of assemblies.

2021-10-06T23:56:51Z

Summary


Details

Preparing to migrate Solid Edge data into a Teamcenter managed environment. Are Families of Assemblies  supported? When they are being migrated, an Item Number is only assigned to the top level and not the members in the Family.



Solution

Review help documents at:  http://docs.plm.automation.siemens.com/tdoc/se/2020/se_help/#uid:xid1516913   for details. 

This is correct behavior. Once the master FOA has been added, each member will be added as its own Item Number at the time the member is published when working within Solid Edge using SEEC.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1903
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: DATA_PREP

Ref: 001-9679476

KB Article ID# PL8017014

Contents

SummaryDetails

Associated Components