PSTC - Unable to Edit the Group in Process Simulate

2021-10-07T00:01:52Z

Summary


Details

- In MPP, highlight the desired process structure, right-click -> Open with Process Simulate 
- In PSTC, highlight two of the resources (or parts), right pick -> Create Group 
- In the 'Create Group' interface, 'Name' the group accordingly, and then pick OK 
- On the 'Logical Collections Tree' tab, see that the Group has been created successfully 
- At this point, the user has realized that he forgot to add one additional resource or part to the newly created group. Highlight the Group, right pick -> ...see that there is no option to 'Edit Group' 
*** NOTE: For the user to include the additional part/resource, he must 'Delete' the Group, re-select all the necessary items, and then create a brand-new Group. This is especially problematic when the user has created a large grouping and only needs to include one additional item. 



Solution

It is possible to Add and Remove objects from a Logical Collections Group without an "Edit Group" command. 
To Add to a Group, just drag and drop from the Object tree into the Group. 



To remove from a Group, right-click on the Group member, and Delete. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V15.0.1.X
Function: UI

Ref: 001-3058579

KB Article ID# PL8017012

Contents

SummaryDetails

Associated Components