Solid Edge Assembly dataset Named References contains multiple SE_Attr0 entries.

2021-10-06T23:56:50Z

Summary


Details

Why are their duplicate entries called SE_Attr0 in the Assembly Name Reference?



Solution

The SE_attr0 object is a form.  SEEC uses the property on the form to track if the assembly was last saved as a simplified assembly (value=1)  or not (value=0).

It is safe to remove duplicate SE_Attr0 objects from the Name Reference.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: P219.0
Function: SEEC

Ref: 002-8016963

KB Article ID# PL8016963

Contents

SummaryDetails

Associated Components