NX Mill Turn Post to output the spindle preselect

2021-10-06T23:27:35Z
NX for Manufacturing

Summary


Details

What TCL code can be used to check to see if the Preset Spindle RPM is set in Post Builder and if so to output it?



Solution

The following Custom Command can be added to both the Initial Move and the First Move in Post Builder to output this value.


### 
global mom_spindle_preset_rpm 
global mom_spindle_preset_rpm_toggle


if { [info exists mom_spindle_preset_rpm_toggle] && $mom_spindle_preset_rpm_toggle == 1 } { 
 MOM_output_literal "G97 S$mom_spindle_preset_rpm" 
} else { 
 set mom_spindle_preset_rpm 0 

###



Notes and References

Please be aware that any code provided by GTAC is intended to be used for sample purposes only. It is the user's responsibility to determine whether the code is suitable for the purpose.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1903
Function: POSTBUILDER

Ref: 001-9679719

KB Article ID# PL8016958

Contents

SummaryDetails

Associated Components

Manufacturing Post Builder