NX Monthly Update is available for download

2021-10-07T00:08:49Z

Summary


Details


Dear Siemens Customer,
 
We are pleased to inform you that the latest product release of NX is now available for download from the Siemens PLM Download Server.
 
Download of NX on Windows 64-bit
   
Please use the following steps to download the NX product release and its documentation.
Note: A valid WebKey account is required. 



  • In your browser's address field enter the URL: https://download.industrysoftware.automation.siemens.com/
     
                           Login using your WebKey username and password
     
  • From the Download page, enter "SiemensNX-1904_wntx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages.  
        
  • Alternatively, the NX product release can be found using file navigator by entering NX into the Product Filter Feature on the left of your browser and then navigating through the NX directory structure as follows:  
    • Expand the "NX" folder 
    • Expand the "NX 1899 Series" folder 
    • Expand the current release folder (NX 1904)   
        
        
  • Note:  When a version is replaced by a newer version, the previous version will be moved to the "NX Support" folder.  For example, when NX 1899 is replaced, it can be downloaded as follows:  
    • Expand the "NX Support" folder 
    • Expand the "NX Supported" folder 
    • Expand the "NX 1899 Series" folder 
    • Expand the available release name 
  • To download the NX product:     
    • Right click on the Release Package files 
    • Select "Save Target As" or "Save Link As" to save the files to your local destination 
  • Note: There are two options to download NX. The first option is recommended for customers running the most recent versions of NX 1899. To upgrade, download the following file and double click to begin the installation program. Automatic updates are currently available. 
    • SiemensNX-1904_wntx64_MSP.zip 
 
  • The second option is recommended for customers who do not have a previous NX 1899 Series release installed. 
    • SiemensNX-1904_wntx64.zip 
 
Please refer to the readme file with the download for instructions on extracting the main zip file.
 


  • To download the NX documentation:  
    • Expand the "NX Support" folder 
    • Expand the "NX Supported" folder 
    • Expand the "NX 1899 Series" folder 
    • Expand the "NX 1899" folder 
    • Expand the "Documentation" folder 
    • Right click on the product documentation link 
    • Select "Save Target As" or "Save Link As" to save the file to your local destination. 
In all cases, please refer to the supplied README file for installation instructions.
 
If you encounter any problems during this installation, please contact your local Siemens PLM Software support office.
   
For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:
   
             http://www.plm.automation.siemens.com/en_us/products/nx/
             http://support.industrysoftware.automation.siemens.com/gtac.shtml 

  

Sincerely,
 
 
Siemens Digital Industries Software 

SFB-NX-8017112
Product Information:
  • Product: NX

KB Article ID# PL8017112

Contents

SummaryDetails

Associated Components