In the Add Reuseable Component dialog, if you have different Parameters in the below order:
Type: Metric or Inch, Screw Type, Thread Type, Length
Low Head: Yes or No
Self Locking: Yes or No
If you want to set Self Locking and Low Head before seeing the other parameters, how can you do it?
Solution
From Reuse Library -> Select Create/Edit KRX file:

To move "Self_Locking" in the KRX file dialog -> selecting the parameter and then use the "Up/Down" arrow to desired order.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: KDA
Version: V12.0.2
Function: REUSE_LIBRARY
Ref: 001-9674215