When saving Solid Edge files into Teamcenter a warning is returned, "The instance is not locked". After dismissing the message the file is saved into Teamcenter with no apparent problems.
Solution
The message can be returned if Teamcenter attributes are misspelled in attribute mapping. Verify that the spelling of the Teamcenter attribute real name in the mapping matches exactly with the real name on the Teamcenter attribute.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP4
Function: SEEC
Ref: 001-9671783