TC 11.6.0.5
NX 12
Desription:
From TC MPP using attachment to select the UGMaster to send to NX, once loaded in NX Line Designer, notice sub-assembly is not loaded, when attempt to check it on to load, it unchecks itself and will not load.
Upon further review in NX by activating the assembly navigator, it shows those unloaded components are in "Suppression" state, meaning they are suppressed. Now, whenever a component is suppressed, it will not load in NX..
However, MPP shows these components.
Solution
The structure in TC (MPP) was configured by Effectivity.
In NX for Line Designer, it is required to go to Assembly Load Options and in this case select "Edit Effectivity" in order to configure the same way as Teamcenter.
After this action was performed, the assembly loaded in Line Designer as expected.
Hardware/Software Configuration
Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: MFG_LINE_DESIG
Version: V12.0.1
Function: GENERAL
Ref: 002-8016893